Our range of precision fasteners benefit from being manufactured in-house at our Chichester site. Our CNC lathes are working day and night to produce our wide array of shoulder, captive, sealing and vented screws in many sizes and materials, including PEEK. Not only does this allow us to reduce lead times it means we can bring products closer to the people and businesses that need them.
By supplying components locally, we can also help reduce transport distances,
whilst supporting UK-based manufacturing.
As part of our commitment to making sustainable choices across our operations, in-house manufacturing sits alongside our other initiatives such as renewable energy, packaging, recycling and waste management.
Our range of precision fasteners benefit from being manufactured in-house at our Chichester site. Our CNC lathes are working day and night to produce our wide array of shoulder, captive, sealing and vented screws in many sizes and materials, including PEEK. Not only does this allow us to reduce lead times it means we can bring products closer to the people and businesses that need them.
By supplying components locally, we can also help reduce transport distances,
whilst supporting UK-based manufacturing.
As part of our commitment to making sustainable choices across our operations, in-house manufacturing sits alongside our other initiatives such as renewable energy, packaging, recycling and waste management.
PEEK (Polyether Ether Ketone) is an advanced engineering thermoplastic developed for applications where unique material properties are required. Offering excellent strength, exceptional chemical resistance and
outstanding thermal stability, PEEK fasteners are specified across industries where reliability, cleanliness and durability are essential.
It’s unique balance of properties makes PEEK particularly valuable in medical equipment, food processing machinery, electronics, aerospace and other regulated manufacturing environments.






Shoulder screws, also known as shoulder bolts or sometimes referred to as stripper bolts, distinguish themselves by featuring a head, a threaded portion, and an additional unthreaded “shoulder” in between. This shoulder, with a larger diameter than the thread and high precision tolerance, serves a dual purpose as both a fastener and a precise guide for moving parts. Available in various materials, including stainless steel and titanium, shoulder screws offer versatility and reliability in applications requiring precise alignment and support for moving components.
Captive screws, designed for permanent hold or “captivation,” offer enhanced safety by significantly reducing the likelihood of accidental removal once installed. The reduced diameter section of the screw helps keep the screw captivated in the panel once the panel has been removed, hence the name.
This captivation is crucial for compliance with safety regulations, such as the EU Machine Safety Directive (2006/42/EC) and/or ISO 14583, where certain equipment, like safety covers or panels, require permanent fastenings.
Sealing screws offer crucial bi-directional protection against contaminants, preventing potential damage to sensitive devices. Featuring an O-ring beneath the screw or bolt, these screws create a reliable seal as they are tightened, controlled by a precision engineered groove. This design ensures consistent O-ring compression, making the screws reusable.
Various O-ring materials resist diverse chemical and environmental conditions. Sealing screws, available to military specifications (MILSPEC) on request, are user-friendly, requiring no special preparation or re-tightening
Vented screws are purpose-built for applications where trapped air bubbles pose challenges, such as in vacuum systems and clean rooms. The vent allows trapped air under the screw to be released quickly. Therefore, systems that are subjected to vacuum conditions can reach low pressures more quickly and remain at low pressures more effectively.
All products are ultrasonically cleaned to meet the cleanliness requirements of vacuum environments. Additionally, coatings are offered to reduce seizing or galling in vented screws.
Low head screws, crucial in weight-sensitive applications like aerospace, provide minimal weight and reduced drag. Unlike traditional countersunk screws requiring a minimum metal depth for head recess, our innovative low head profile screws allow for the use of thinner panels, saving weight and ensuring a flush fit with the surface, with thicknesses as minimal as 0.5mm. Available in hex or TX versions, these screws provide a streamlined solution for applications requiring both lightweight design and reduced aerodynamic resistance.
Company registration no: 00496138
Company VAT number GB 408154022
Alexia House, Glenmore Business Park
PO19 7BJ Chichester
United Kingdom
0333 207 4498
sales@automotioncomponents.co.uk